AXIS#.MOTOR.LDLL
Description
This parameter is the motor line to line direct (flux producing) axis inductance.
-
- This parameter is automatically configured for Kollmorgen motors when AXIS#.MOTOR.AUTOSET = 1 and can be modified while AXIS#.MOTOR.AUTOSET = 1 if its AXIS#.MOTOR.DISAUTOSET index = 1.
-
-
This parameter is required to be configured for AXIS#.MOTOR.TYPE = 0, 1, 4, 6, and 8.
Context
For more information see Motor.
Versions
| Action | Version | Notes |
|---|---|---|
| Implemented | 02-00-00-000 |
General Information
|
Type |
Read/Write |
|
Units |
mH |
|
Range |
1 to 2^31 |
|
Default Value |
4 |
|
Data Type |
Float |
|
Stored in Non-Volatile Memory |
Yes |
Variants Supported
All variants are supported.
Fieldbus Information
|
Command |
Index |
SubIndex |
Data Type |
Units |
Float Scale |
Access |
PDO Mappable |
|---|---|---|---|---|---|---|---|
|
AXIS1.MOTOR.LDLL |
500bh |
28h |
Unsigned32 |
- |
1000:1 |
Read/Write |
No |
|
AXIS2.MOTOR.LDLL |
510bh |
28h |
Unsigned32 |
- |
1000:1 |
Read/Write |
No |
|
ID |
Instance |
Attribute |
Name |
Data Type |
Access |
User Mappable |
|---|---|---|---|---|---|---|
|
6230 |
1 |
6230 (0x1856) |
AXIS1.MOTOR.LDLL |
Unsigned32 |
Read Only |
Yes |
|
71766 |
2 |
6230 (0x1856) |
AXIS2.MOTOR.LDLL |
Unsigned32 |
Read Only |
Yes |
|
Parameter |
PNU |
Data Type |
Access |
Units |
|---|---|---|---|---|
|
AXIS#.MOTOR.LDLL |
6230 |
Float |
Read Only |
- |